Does the EdgeLock SE050 Plug & Trust middleware support non NXP MCU / MPU boards?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does the EdgeLock SE050 Plug & Trust middleware support non NXP MCU / MPU boards?

2,484件の閲覧回数
jordijofrenxp
NXP Employee
NXP Employee

The EdgeLock SE050 Plug & Trust middleware comes with pre-built support for many NXP MCU / MPU boards. However, you can also leverage SE050 Plug & Trust middleware if you are using any other MCU / MPU board.

From an HW perspective, you can use the OM-SE050ARD evaluation board to connect your board via the Arduino connectors or the external I2C connector.

From an SW perspective, The EdgeLock SE050 Plug & Trust middleware has been designed to facilitate portability to multiple platforms and OS. For more information about how to port the middleware, you can refer to AN12448 SE050 Plug & Trust middleware porting guidelines.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,496件の閲覧回数
rodolfoveltrigo
NXP Employee
NXP Employee

Hi all,

this is the new NXP weblink of this application note (old link does not work anymore).

https://www.nxp.com/docs/en/application-note/AN12448.pdf

Cheers

Rodolfo

0 件の賞賛
返信