A71CH and TLS 1.3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

A71CH and TLS 1.3

2,223件の閲覧回数
antoniosantagiu
Contributor I

Hello

will the A71CH support TLS version 1.3 ? I can read that currently the chip support TLS 1.2.

More in general, can this chip be upgraded to follow new TLS releases once installed ?

Let's say, what happens when a vulnerability is discovered on TLS 1.2 implementation?

thank you

ラベル(1)
0 件の賞賛
返信
1 返信

2,064件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi,

Yes, it supports. Actually limiting factor here is just the version of OpenSSL which we have in our PSP code. With the crypto capabilities of the A71CH also TLS 1.3 authentication have to be possible.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信