update S32R274 FMEDA

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

update S32R274 FMEDA

698件の閲覧回数
zhiqiang_huang
Contributor I

    The FMEDA of S32R274,the version I got is :Rev. 1.3/2017-11-23.

Please help to get the new version to make sure:The results of self-verification are inconsistent with the data provided.

zhiqiang_huang_1-1629802193867.jpeg

タグ(1)
0 件の賞賛
1 返信

592件の閲覧回数
nxf64307
NXP Employee
NXP Employee

Hello,
The mentioned version is indeed the latest version that we have for S32R274 device. The inconsistency which you have observed in the metrics is intentional so as to avoid the misinterpretation of achieved FMEDA results. We have added a DC Limiter function which blocks the FMEDA result to limit the metric to the shown value even though the achieved random hardware fault metric is exceeded than the required target value. This is done as NXP is not claiming systematic coverage greater than the target ASIL mentioned in FMEDA.

In this case SPT and Performance cores are not expected to provide systematic coverage more than ASIL B target and hence a limiter is blocking these values to 96.9 so that the end user does not use these modules for applications required to achieve greater than ASIL B.

0 件の賞賛