S32V234 Safety questions

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32V234 Safety questions

671 Views
Daniel_Wax
NXP Employee
NXP Employee

I have a customer I am helping with changes to FMEDA assumptions and we have these questions.

 

Currently we will be only modifying CORE and RAM FMEDA

 

 

FMEDA

Column

Question

Response

Core

 

AR3 - TVF’s

Are TVF’s enabled by Default

 

T3- STM/PIT

How to enable STM/PIT using QNX has it been done before any sample code?

 

K3 - ITM

How to enable ITM - sample code? Impact of disabling it?

 

AS3 - Parity Protection Interconnect

 

Is this referring to the MEW which is capable of embedding ECC/EDC in the data

 

RAM

AB3 - CRC static data for MMDC0

Are we referring to Static configuration registers?

Does this have to use the CRC hardware onboard the S32V? What is the impact if we use a software implementation?

What if - Alternatively, we can check the register contents completely

 

AG3 - CRC static data for MMDC1

Are we referring to Static configuration registers?

 

 

AE3-ECC for MMDC1 (- not possible on cut1-

ECC on MMDC1 not possible? Could you explain?

 

Labels (1)
0 Kudos
1 Reply

655 Views
nxf64307
NXP Employee
NXP Employee

Hello Daniel,

I hope the above query was answered over email and is clarified. Please do let me know if you have any query further associated to this. 

Also, attached the Table below with the response.

FMEDA

Column

Question

Response

Core

 

AR3 - TVF’s

Are TVF’s enabled by Default

yes, they are enabled always.

(The FMEDA allows to disable this feature but in HW it is always enabled).

T3- STM/PIT

How to enable STM/PIT using QNX has it been done before any sample code?

The question is unclear. The FMEDA asks whether the

“System Timer (STM) is safety relevant”.  That may or may not be the case in a particular application.

If yes, the errors are calculated, otherwise they are considered safe.

K3 - ITM

How to enable ITM - sample code? Impact of disabling it?

The INTM is only available for 4 interrupts which are critical for the application. The impact can only be judged on system level. The S32V234 as such works fine without INTM. The only impact is that potential interrupt handling errors might not be detected.

AS3 - Parity Protection Interconnect

 

Is this referring to the MEW which is capable of embedding ECC/EDC in the data

This is not related to MEW.

This is related to the EDC used on:

  • Main Interconnect NIC-301
  • Cache-coherent interconnect  CCI-400
  • Crossbar Switch (AXBS)

 

Note: This is not related to protection of interconnect which is inside HPSMI. This is analyzed in the respective RAM FMEDA.

RAM

AB3 - CRC static data for MMDC0

Are we referring to Static configuration registers?

Does this have to use the CRC hardware onboard the S32V? What is the impact if we use a software implementation?

What if - Alternatively, we can check the register contents completely

The CRC is over the content stored in DRAM.

The Fast_DMA has been designed for this purpose and is probably the fastest check and simplest implementation. However, any other check (e.g. by SW) of the content in DRAM can be used alternatively (CRC or direct comparison, etc ...). Please keep in mind that the SW executing the test may be impacted by the fault it is trying to detect (if running from code in that DRAM).

If ECC is used, this CRC may not be required. If no ECC is used, it depends on the usage of the DRAM content whether such test is required or not.

 

The check of static configuration registers is configured in column AN.

AG3 - CRC static data for MMDC1

Are we referring to Static configuration registers?

 Same as above.

 

AE3-ECC for MMDC1 (- not possible on cut1-

ECC on MMDC1 not possible? Could you explain?

Cut1 has only one DRAM controller equipped with ECC: This has been changed from cut2 onwards. The comment “(- not possible on cut1” can be ignored and AE5 can be enabled (if ECC is used).

 

Regards,

Rupesh

0 Kudos