In “P2210052M_0_0 General Market S32K344 Global Foudnries Fab-7 P55A 172MAXQFP PPAP.pdf” which can be found in Safe Assure NDA, you can find list of TUE (ADC Total Unadjusted Error)@5V and 3V in p4836.
In this document two different TUEs are listed for each voltage.
Would you please confirm what is difference between top and bottom?
Hi Kuniyaki,
It was confirmed with the IP onwer that TUEP is the maximum positive error and TUEN is the “maximum” negative error (greatest deviation to the negative side from ideal). TUE is basically the umbrella of it. The TUEN/TUEP is a testing thing so to say.
We have a constructed offset effect due to the fact that the VREFL signal does not come privately out of the chip and is shared with analog ground. The current flowing on analog ground is offsetting
the reference as the ADC sees it which makes the TUE curve skewed a bit (which is also the case why the very small package where a further ground is shared has a less good TUE spec). This is why it was TUEP is worse than TUEN.
Hope this helps !
Thanks