[Medini files]S32K3xx customized FMEDA

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[Medini files]S32K3xx customized FMEDA

ソリューションへジャンプ
2,000件の閲覧回数
BoxLi
NXP Employee
NXP Employee

Hi:

Just want to confirm that whether we could release K3xx fmeda Medini file to customer?

  • If yes, does MediniAnalyze version must be 2021 R2?
  • If yes, could be via secure file or other ways?

My customer baught Ansys Mediti tool already, they want to make FMEDA with their own configuration.

Thanks a lot.

 

ラベル(1)
タグ(1)
0 件の賞賛
1 解決策
1,972件の閲覧回数
Yashwant_Singh
NXP Employee
NXP Employee

Hello,

Yes the medini files for the S32K3xx family are available upon requests. Ansys release different version each year so the .mprx files for different products in the family are available under different versions however Medini allows migrating files to newer versions of the tool and so we would recommend using the latest one (2023 r2 or newer).

Secure files is the official channel for release however it can also be done via a common sharepoint link or drive with the customer.

Thanks!

-Yashwant

 

 

元の投稿で解決策を見る

0 件の賞賛
2 返答(返信)
1,973件の閲覧回数
Yashwant_Singh
NXP Employee
NXP Employee

Hello,

Yes the medini files for the S32K3xx family are available upon requests. Ansys release different version each year so the .mprx files for different products in the family are available under different versions however Medini allows migrating files to newer versions of the tool and so we would recommend using the latest one (2023 r2 or newer).

Secure files is the official channel for release however it can also be done via a common sharepoint link or drive with the customer.

Thanks!

-Yashwant

 

 

0 件の賞賛
1,952件の閲覧回数
BoxLi
NXP Employee
NXP Employee

Hi Yashwant:

Got it, thanks a lot.

0 件の賞賛