MPC5746C FMEDA for customer use case

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5746C FMEDA for customer use case

462件の閲覧回数
viktorfellinger
NXP Employee
NXP Employee

Dear support,

customer Bosch is  observing a FCCU state transition failure after the reset due to FCCU FLL fault and as a solution they will be performing destructive reset if any FCCU fault is identified.

But they  have a software where, the destructive reset implementation solution is not applied. In that software the reset’s will be in loop till the FCCU FLL fault recovers. FCCU can capture 72 faults as mentioned in the reference manual. So they request to generate a customer tailed summary FMEDA where fault mentioned as not "sure are" below are not considered for the FMEDA

viktorfellinger_0-1733133624435.png

 

 Best Regards,

Viktor

ラベル(1)
0 件の賞賛
1 返信

439件の閲覧回数
antoinedubois
NXP Employee
NXP Employee

HI Viktor, I have emailed you separately on this issue. We do not provide Customized FMEDA, but we can support customer to do it on their own.

Antoine

.

 

0 件の賞賛