EIM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

EIM

896 次查看
HeebeomPark
Contributor II

Once the safety manual is updated to 6.0, there are some comments for configuration as below in the red box.

Is it only information or what should the user do for this?

HeebeomPark_0-1739182352161.png

 

HeebeomPark_1-1739182370696.png

 

 

0 项奖励
3 回复数

734 次查看
antoinedubois
NXP Employee
NXP Employee

Hi Heebeom, SM2 usually inject failure using the EIM interfaces (not always). If you use NXP SAF Scheck (recommended), you do not need to implement anything else, EIM fault injectino is transparent to you.

0 项奖励

811 次查看
john_floros
NXP Employee
NXP Employee

Hello,

The user needs to do the error injection to be sure that the ECC check is working.

Regards,

John

0 项奖励

792 次查看
HeebeomPark
Contributor II

Normally, SM2(es) are supported to check the functionalities of checkers.

In terms of the purposes, instead of using the SM2 can be sufficient at least for ECC and Gasket and so on?

0 项奖励