Customizable FMEDA for 5777C

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Customizable FMEDA for 5777C

652 次查看
MarceloNXP
NXP Employee
NXP Employee

Hello,

Can you please help me with this request from our customer? They need an FMEDA that can be customized, not the static ones for the 5777C

“The big issue we’re having right now is that the MPC5777 FMEDA you sent to us is a static FMEDA and does not contain conditional formulas, so it cannot be customized/utilized. It does appear that enabling / disabling of safety features is allowed in the spreadsheets but the results are not recalculated they are static. Based on MPC5777 FMEDA report part 1 (page 16) we need the “internal FMEDA” which can be tailored to our application.”

Thank you!

Thank you!

0 项奖励
1 回复

649 次查看
naveenm
NXP Employee
NXP Employee

Hi Marcelo,

For customers only static FMEDA is published. Since customer is asking for re-configuration of FMEDA to support their use-case. The action is on FAE community to support (shown in the red box below). 

naveenm_0-1645591102623.png

Let me know if there are any questions.

Regards,

NaveenM

0 项奖励