Cobra-55 asil-d inter-processor communication

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cobra-55 asil-d inter-processor communication

1,916 Views
lorenzodaniele
NXP Employee
NXP Employee

Hi,  customer Marelli Powertrain is asking for some comments/guidance on the architecture upgrade described in attached file.

Looking for a safety expert contact to continue the discussion

Thanks

2 Replies

1,851 Views
janna_garofolo
NXP Employee
NXP Employee

Hi Lorenzo,

Can you please provide feedback from Marelli on whether this information allowed them to determine the architecture for their system?  Also, can you please share the architecture decision that was made by Marelli?

Thank you,

Janna

0 Kudos

1,851 Views
sandeepkumarbom
NXP TechSupport
NXP TechSupport

Hi Lorenzo,

Please let me know my understanding is correct for the below image as per your description.

The requirement proposed by FCA is very much an ASIL D requirement. But the implementation proposal cannot meet ASIL D by itself. As you see, the implementation is very much dependent on eDMA to transfer data from RAM to SIPI. Any error in eDMA to write data to SIPI would lead to deactivation of both the motors.  I would suggest having additional checks to make sure the eDMA is sending data in a timely manner and there is a proper acknowledgment on SIPI. As eDMA is not replicated that totally doesn’t mean it cannot send safety critical data. As long the Safety software is implemented to make sure there are additional checks implemented like a checker to checker failsafe, this can meet ASIL D.

 

In this Scenario, an Additional check can be having an additional communication link between the two MCUs like sending the angular position information over CAN (just an example) and comparing it to the data received over Zipwire. Also, if the application has wheel speed sensors, master MCU can compare Speed on rear wheels not by just judging the data over Zipwire. There can be multiple ways this we can look at.

Capture.JPG