Issues Flashing Bootable Image to S32Z270-DC Board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Issues Flashing Bootable Image to S32Z270-DC Board

1,248 次查看
raz3l
Contributor III

Hi everyone,

I'm having some issues flashing a bootable image to the S32Z270-DC board. Here’s the current setup and the steps I’ve followed:

  • S32 Design Studio v3.6.2

  • Lauterbach debugger (working fine for debugging)

  • Using SMU-CM33 core

  • Target: blinking the D12 LED as a basic test

Steps I’ve taken so far:

  1. Generated a .bin file

    • I modified the project settings to generate a binary file from the LED example. 

  2. Created an IVT image using the S32 IVT Tool

    • Selected the LED example application (which works when debugged via Lauterbach).

    • This is the configuration:

image1.pngimage2.png

  • After configuration, I pressed the "Export Image" button in the Application Bootloader section to update the image blob.

  1. Flashing the image

    • In the IVT tool, I clicked "Flash Image" and selected the S26HS512.bin algorithm for HyperFlash.

    • Issue: The flashing process is inconsistent. Sometimes it succeeds, but often it fails.

    • I noticed slightly better results after disconnecting the Lauterbach JTAG adapter, but the success rate is still not reliable.

  2. Board boot configuration

    • After (successful) flashing, I changed the RCON switches to 0x70481804, which I copied from the HyperFlash Lauterbach script.

    • I then power-cycle the board.

 

After flashing and power-cycling, I expect the D12 LED to blink (as it does when I run it from the debugger), but nothing happens.

Is there anything I'm missing in all of this process? Could the RCON value be incorrect?

 

Any help or tips would be much appreciated! Thanks in advance.

标记 (3)
0 项奖励
回复
3 回复数

1,242 次查看
raz3l
Contributor III

The error that I'm getting all the time from the flash tool.

raz3l_0-1752078886470.png

 

0 项奖励
回复

1,222 次查看
raz3l
Contributor III

I have also tried to flash to the QSPI Flash by connecting to the J119 USB with this configuration:

RCON switches:

raz3l_0-1752169484750.png

J1245 and J125 in serial mode:

raz3l_1-1752169595043.png

I got the same error with the Flash Tool:

raz3l_2-1752169721660.png

 

Am I doing anything wrong?

 

 

 

0 项奖励
回复

1,214 次查看
alejandro_e
NXP TechSupport
NXP TechSupport

Hello @raz3l,

Sorry for the late reply. It seems that there was a problem in our internal ticket tracking tool and this post did not get a ticket number and therefore cannot be assigned to one of our support engineers. If possible create a new post, you can explain this problem and just reference the link to this post, this should create an internal ticket and one of my colleagues should help you.

I will report this problem so that it does not happen again.

I apologize for the inconveniences.

 

Thanks