'Synchronous Abort' during boot on S32V

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

'Synchronous Abort' during boot on S32V

3,253 次查看
erezsteinberg
Contributor IV

Hello experts,

I am trying to boot S32V234 (28899 Rev D) from SD-Card.

I used 'fsl-image-auto-s32v234evb28899.sdcard' from binary_auto_linux_bsp16.0

Boot gets stuck in a loop with the following output:

U-Boot 2016.01+ge19ad21 (Mar 03 2018 - 03:54:13 +0700)
CPU:   NXP S32V234 V1.0 at 1000 MHz
Reset cause: Software Functional reset
Board: s32v234evb29288
I2C:   ready
DRAM:  "Synchronous Abort" handler, esr 0x96000010
ELR:     3e827dec
LR:      3e847c60
x0 : 000000007fd6cf68 x1 : 000000003e8558ad
x2 : 0000000080000000 x3 : 000000003e827dd8
x4 : 000000007fd6d000 x5 : 0000000000000013
x6 : 0000000000000098 x7 : 0000000020000000
x8 : 00000000fffffffe x9 : 000000000000000c
x10: 00000000ffffff7f x11: 000000003ebdfa8f
x12: 00000000ffffffff x13: 00000000ffffffff
x14: 0000000080000000 x15: 0000000080010000
x16: 000000003e82249c x17: 30a000008600d000
x18: 000000003ebdfca0 x19: 000000003e85d030
x20: 000000003e85cf28 x21: 0000000000000000
x22: 260628080000840a x23: 00418090100000a0
x24: 0001810220000041 x25: 10d0080000008000
x26: 4083424004020012 x27: 00c3207010000000
x28: 0654729000000000 x29: 000000003ebdfc50
Resetting CPU ...
resetting ...

Any suggestions how to proceed?

Regards,

Erez

标记 (1)
0 项奖励
回复
1 回复

2,915 次查看
KushalShahNXP
NXP Employee
NXP Employee

Hi Erez,

From the information you provided it seems that you are using fsl-image-auto-s32v234evb28899.sdcard image. While error message shows the s32v234evb29288 board. Both are different boards

Can you please check if you are using correct image with correct board?

Kushal

0 项奖励
回复