@NXP I need the official OV camera module's lens parameters to confirm whether it meets our project requirements.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

@NXP I need the official OV camera module's lens parameters to confirm whether it meets our project requirements.

1,685 Views
quguipeng
Contributor I

The attached picture is the official OV module.our project need the front view camera module ,which the horizontal field angle is between 50 and 60 degrees ,the vertical field angle is between 30 and 40 degrees. could you please help me with offerring the OV10640CSP-S32V camera module lens parameters?

Tags (1)
0 Kudos
Reply
1 Reply

1,483 Views
KushalShahNXP
NXP Employee
NXP Employee

Hi Qu,

The OV10640CSP-S32V is the MIPI based camera module with Sunex DSL219 lens. Which is a Fisheye lens. This is the same camera module as OV10640-EAAG-AA01 and is manufactured by Omni-Vision. Please contact Omni-Vision to inquire about all available options and more specifications.

Regards,

Kushal

0 Kudos
Reply