S32Vナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32V Knowledge Base

ラベル

ディスカッション

ソート順:
Index | Previous | Next
記事全体を表示
Index | Previous | Next This video goes over the Apex Architecture showing what makes it different from other solutions
記事全体を表示
SOFTWARE The S32 Design Studio for ARM® The S32 Design Studio for Vision The Vision Toolbox for MATLAB® The Automotive Ethernet Audio Video Bridging (AVB) HARDWARE The SBC-S32V234 evaluation board The S32V234-EVB2 evaluation system The NXP Blue Box Autonomous Driving Development Platform TOOLS NEXT TOPIC
記事全体を表示
The S32V234 is our 2nd generation vision processor family designed to support computation intensive applications for image processing and offers an ISP, powerful 3D GPU, dual APEX-2 vision accelerators, security and supports SafeAssure™. S32V234 is suited for ADAS, NCAP front camera, object detection and recognition, surround view, machine learning and sensor fusion applications. S32V234 is engineered for automotive-grade reliability, functional safety and security measures to support vehicle and industrial automation. S32V234 has a complete enablement platform supported by S32 Design Studio IDE for Vision which includes a compiler, debugger, Vision SDK, Linux BSP and graph tools. Video Link : 8296 The target applications for S32V234 are: Automotive Sensor Fusion Systems Automotive Vision Systems Front View Camera Intelligent Roadside Unit Smart  Rear-View Camera Surround View & Sense Park Assist System Surround View Park Assist System NEXT TOPIC
記事全体を表示
WHAT YOU WILL LEARN: Understand the basic aspects of S32V234 vision processors, the second generation vision MPU family for supporting computation intensive applications for image processing 1.1 S32V overview High-level overview Target applications 1. 2 S32V enablement Software Hardware Tools
記事全体を表示
Hi, I am currently working on SPI with DMA for S32V234. I have tested SPI code it is working fine. I am tested for SPI1 and chip select 0 and mode 3 it is working fine. Now i have to implement SPI with DMA code. Please see the below links i have taken as a reference for s32v234, I made little bit changes in that link source code. http://lists.infradead.org/pipermail/linux-arm-kernel/2014-February/235598.html https://www.toradex.com/community/questions/1961/vf61-linux-spi-dma-support.html 1. Can you please suggest which link is suitable for s32v234? 2. How to write dtsi for "spi with dma"? I wrote the below lines, when compiled it's getting error?      spi1: spi@400C0000 {                                 compatible = "fsl,s32v234-dspi";                                 reg = <0x0 0x400C0000 0x0 0x1000>;                                 interrupts = <0 62 4>;                                 clocks = <&clks S32V234_CLK_SYS6>;                                 clock-names = "dspi";                                 spi-num-chipselects = <4>;                                 bus-num = <1>;                                 spi-cpol;                                 spi-cpha;                                 /* TODO: Update the dma when edma ip is activated*/                                 use-dma;                                 dmas =  <&edma 12>,                                         <&edma 13>;                                 dma-names = "rx","tx";                                 status = "disabled";                 }; ERROR (phandle_references): Reference to non-existent node or label "edma" ERROR (phandle_references): Reference to non-existent node or label "edma" ERROR: Input tree has errors, aborting (use -f to force output) scripts/Makefile.lib:293: recipe for target 'arch/arm64/boot/dts/freescale/s32v234-evb.dtb' failed make[2]: *** [arch/arm64/boot/dts/freescale/s32v234-evb.dtb] Error 2 scripts/Makefile.build:403: recipe for target 'arch/arm64/boot/dts/freescale' failed make[1]: *** [arch/arm64/boot/dts/freescale] Error 2 arch/arm64/Makefile:89: recipe for target 'dtbs' failed make: *** [dtbs] Error 2 3. Please give do you have any reference code SPI with DMA for S32V234. I am waiting for your reply. Thanks & Regards, Ramanjineyulu.
記事全体を表示
Index | Previous | Next
記事全体を表示
Index | Previous | Next This video will present the high level ISP architecture in the S32V234 with some background information.
記事全体を表示
Index | Previous | Next This video introduces the concepts of Image Signal Processing for cameras like the ones typically applied to Raw camera data and that could be implemented in the S32V234 ISP.
記事全体を表示
Index | Previous | Next
記事全体を表示
Index | Previous | Next
記事全体を表示
Index | Previous
記事全体を表示
Index | Previous | Next
記事全体を表示
Index | Previous | Next
記事全体を表示
Index | Previous | Next
記事全体を表示
Index | Previous | Next Video goes on detail regarding the APU (Kernel) programming
記事全体を表示
Index | Previous | Next
記事全体を表示
Index | Previous | Next This video provides a quick summary of the previously studied concepts regarding the Apex and image processing 
記事全体を表示
Index | Previous | Next
記事全体を表示
Index | Previous | Next Explains the three main components of creating a kernel: Implementation, Metadata and Wrapper.
記事全体を表示