Hi, I am currently working on SPI with DMA for S32V234. I have tested SPI code it is working fine. I am tested for SPI1 and chip select 0 and mode 3 it is working fine. Now i have to implement SPI with DMA code. Please see the below links i have taken as a reference for s32v234, I made little bit changes in that link source code. http://lists.infradead.org/pipermail/linux-arm-kernel/2014-February/235598.html https://www.toradex.com/community/questions/1961/vf61-linux-spi-dma-support.html 1. Can you please suggest which link is suitable for s32v234? 2. How to write dtsi for "spi with dma"? I wrote the below lines, when compiled it's getting error? spi1: spi@400C0000 { compatible = "fsl,s32v234-dspi"; reg = <0x0 0x400C0000 0x0 0x1000>; interrupts = <0 62 4>; clocks = <&clks S32V234_CLK_SYS6>; clock-names = "dspi"; spi-num-chipselects = <4>; bus-num = <1>; spi-cpol; spi-cpha; /* TODO: Update the dma when edma ip is activated*/ use-dma; dmas = <&edma 12>, <&edma 13>; dma-names = "rx","tx"; status = "disabled"; }; ERROR (phandle_references): Reference to non-existent node or label "edma" ERROR (phandle_references): Reference to non-existent node or label "edma" ERROR: Input tree has errors, aborting (use -f to force output) scripts/Makefile.lib:293: recipe for target 'arch/arm64/boot/dts/freescale/s32v234-evb.dtb' failed make[2]: *** [arch/arm64/boot/dts/freescale/s32v234-evb.dtb] Error 2 scripts/Makefile.build:403: recipe for target 'arch/arm64/boot/dts/freescale' failed make[1]: *** [arch/arm64/boot/dts/freescale] Error 2 arch/arm64/Makefile:89: recipe for target 'dtbs' failed make: *** [dtbs] Error 2 3. Please give do you have any reference code SPI with DMA for S32V234. I am waiting for your reply. Thanks & Regards, Ramanjineyulu.
查看全文