S32M244 halt CPU problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32M244 halt CPU problem

ソリューションへジャンプ
5,546件の閲覧回数
waldluis
Contributor I
Hello,
 
I am trying to find a way to stop the core of the S32M244 on the S32M24xEVB-L064 evaluation board. I am connected to the board via PJTAG. The plan is to perform a memory mass erase, stop the core, load a RAM bootloader, then start the core to execute the RAM bootloader. The procedure is done as follows:
 
1. Drive reset low 
2. Perform a mass erase with MDM_AP
3. Stop the CPU
    1. Set MDM_CONTROL debug request
    2. Release reset
    3. Stop CPU with DHCSR
    4. Drive reset high
    5. Check if CPU is stopped
    6. Clear the MDM_CONTROL register
4. Drive reset high
5. Load bootloader code into RAM
6. Start bootloader
 
This procedure works in about 60% of the time. Sometimes an error occurs when checking if the CPU is stopped. After that it seems like the connection is broken, because the register readouts all return the same value, which appears to be buffered in the DAP.
Setting the MDM_CONTROL debug request should force the CPU to stop, which doesn't happen. The core can only be stopped by setting the bits in the DHCSR directly.
Has anyone experienced this problem or knows of a straightforward procedure to stop the core without any errors?
タグ(1)
0 件の賞賛
返信
1 解決策
5,508件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @waldluis,

You mentioned these steps:

2. Release reset

4. Drive reset high

4. Drive reset high for the second time.

But the reset is an open-drain pin, it should not be driven high externally.

 

I tested it with this j-link script, and everything works correctly.

// Step 1: Connect
device S32M244
si SWD
speed 4000
connect
sleep 100

// Step 2: Reset
R0
sleep 100

// Step 3: Read MDM_AP
swdwritedp 2, 0x01000000
sleep 100

// Step 4: MDM_AP Status
swdreadap 0  
swdreadap 0
sleep 100

// Step 5: MDM_AP Control
swdreadap 1  
swdreadap 1
sleep 100

// Step 6: Write MDM-AP CONTROL[2] Set to force the core to halt
swdwriteap 1,0x4
sleep 100

// Step 7: Release reset
r1
sleep 1000

// Step 8: MDM_AP Status
swdreadap 0  
swdreadap 0
sleep 100

 

The core is always halted after the reset is released:

danielmartynek_0-1749208218441.png

BR, Daniel

 

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
5,509件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @waldluis,

You mentioned these steps:

2. Release reset

4. Drive reset high

4. Drive reset high for the second time.

But the reset is an open-drain pin, it should not be driven high externally.

 

I tested it with this j-link script, and everything works correctly.

// Step 1: Connect
device S32M244
si SWD
speed 4000
connect
sleep 100

// Step 2: Reset
R0
sleep 100

// Step 3: Read MDM_AP
swdwritedp 2, 0x01000000
sleep 100

// Step 4: MDM_AP Status
swdreadap 0  
swdreadap 0
sleep 100

// Step 5: MDM_AP Control
swdreadap 1  
swdreadap 1
sleep 100

// Step 6: Write MDM-AP CONTROL[2] Set to force the core to halt
swdwriteap 1,0x4
sleep 100

// Step 7: Release reset
r1
sleep 1000

// Step 8: MDM_AP Status
swdreadap 0  
swdreadap 0
sleep 100

 

The core is always halted after the reset is released:

danielmartynek_0-1749208218441.png

BR, Daniel

 

 

 

0 件の賞賛
返信
5,501件の閲覧回数
waldluis
Contributor I

Hello @danielmartynek

Thank you for your quick and helpful response.
I could reproduce your script with the J-Link on my eval-board.
The main difference was the communication speed. I had it set to 1 MHz, which works fine except when stopping the CPU. After changing this for the stop process, this works every time. Is the communication speed specified in any datasheets? It seems to be a crucial factor in the process. The J-Link also fails sometimes at 1 MHz.
With the proprietary device I use, the debug request with the MDM_AP has no effect. The only way to stop the CPU is by modifying the DHCSR directly. I can't explain why, but that's fine as it now works every time.

0 件の賞賛
返信
5,474件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @waldluis,

Yes, SWD and JTAG are specified in the DS, it support higher speeds than 1MHz.

Table 76. SWD electrical specifications

Table 77. JTAG electrical specifications

https://www.nxp.com/docs/en/data-sheet/S32M2xx_DS.pdf

 

Can you use longer wait loops after the swdwrite to the control register and especially after the reset_b release?

 

Regards,

Daniel

 

 

 

0 件の賞賛
返信
5,460件の閲覧回数
waldluis
Contributor I

Hello @danielmartynek

Thank you,
I did some testing with different timeouts after the register write and reset release, but it didn't make much of a difference. Changing to a higher frequency was the big factor, as it made a reliable stop sequence possible.

0 件の賞賛
返信