utest nvm user space programming

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

utest nvm user space programming

Jump to solution
2,500 Views
pasa_kevin_y
Contributor III

is there a way to program utest user space(OTP data) by using jtag direct flashing?

just like how we flash the pflash and dflash?

 

I

0 Kudos
Reply
1 Solution
2,473 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @pasa_kevin_y 

Yes, it is possible. It depends on your tools. If you have Lauterbach debugger, you can use simple script which I shared in this post a few days ago:

https://community.nxp.com/t5/S32K/S32K388-HSE-No-Response-Error/m-p/2090937/highlight/true#M48394

Regards,

Lukas

 

View solution in original post

0 Kudos
Reply
4 Replies
2,474 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @pasa_kevin_y 

Yes, it is possible. It depends on your tools. If you have Lauterbach debugger, you can use simple script which I shared in this post a few days ago:

https://community.nxp.com/t5/S32K/S32K388-HSE-No-Response-Error/m-p/2090937/highlight/true#M48394

Regards,

Lukas

 

0 Kudos
Reply
2,456 Views
pasa_kevin_y
Contributor III

Thanks, it looks like the debugger load a driver to RAM and it plays the magic.

It should also follow the reference manual to program through the registers.

0 Kudos
Reply
2,475 Views
raj12
Contributor III
Hi @pasa_kevin_y,

you can use lauterbach cmm script to write data into UTEST area.
0 Kudos
Reply
2,454 Views
pasa_kevin_y
Contributor III
Thank you for your answer too.
0 Kudos
Reply