the differnence between this two command

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

the differnence between this two command

2,098 次查看
814420552
Contributor III

Hello,

What's the difference between the following erase method?

pastedImage_1.png

I can't get the difference between this two comand,  wish your detail description!!

thanks

0 项奖励
回复
3 回复数

1,993 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi kui wu,

"36.5.9.2 Flash commands" of S32K-RM.36.5.9.2 Flash commands.png

AN12130, Production Flash Programming Best Practices for S32K1xx MCUs - Application Note

AN12130.png

For more detail please read the "37.5.9.11 Erase All Blocks command" and "37.5.9.13 Erase All Blocks Unsecure command" of S32K-RM.

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,993 次查看
814420552
Contributor III

hello, 

   pastedImage_1.png

      when execute this two command it will erase the P-Flash code, If it's erased, isn't it that the application won't run? Need to download the app again。

0 项奖励
回复

1,993 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi kui wu,

If it's erased, the MCU is blank no application run. The reset pin will toggle. Need to download the app again.

Best Regards,

Robin

0 项奖励
回复