select clock for modules with PCC?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

select clock for modules with PCC?

ソリューションへジャンプ
2,216件の閲覧回数
JeorgeB
Contributor III

Hi, 

 

I wanna to use LPSPI. assume there is a SOSC and Core CLK is 80MHz. bus clock is 40MHz. FIRC is 48MHz.

Can I use FIRC as input clock for LPSPI module ? (it is bigger than BUS CLK)

in page 566 for LPSPI, RM says : "Maximum frequency governed by BUS_CLK"

Thanks.

0 件の賞賛
返信
1 解決策
2,176件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

AFigure 51-1. Block Diagram.png

BFigure 10. LPSPI Example Block Diagram.png

CGC low power.png

C. The limitation is for Functional clock, not the clock after divider. Same limitation by using FIRC-48MHz (>40MHz BUS_CLK)

元の投稿で解決策を見る

3 返答(返信)
2,205件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi JeorgeB,

You can not use FIRC(48MHz) as input clock for LPSPI module as it is bigger than BUS_CLK(40MHz).

Maximum frequency governed by BUS_CLK.pngTable 27-9. Peripheral module clocking.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

2,200件の閲覧回数
JeorgeB
Contributor III
Hi Robin, A. what is BUS_CLK role in here? is it only for communication between Master and the module? B. If we gated off this clock [CGC], the module will be switched off (do not consume power)? or we should disable [PCS] clock? C. Assume we, use prescaler and SCK divider with register appropriate setting, and LPSPI SCK clock is 8MHz, is there same limitation by using FIRC-48MHZ? Thanks.
0 件の賞賛
返信
2,177件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

AFigure 51-1. Block Diagram.png

BFigure 10. LPSPI Example Block Diagram.png

CGC low power.png

C. The limitation is for Functional clock, not the clock after divider. Same limitation by using FIRC-48MHz (>40MHz BUS_CLK)