s32k344 CAN bus sample code hard fault issue.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

s32k344 CAN bus sample code hard fault issue.

Jump to solution
2,776 Views
StephenYeh
Contributor III

Hi Sir

I will import the sample code s32k344 CAN bus sample code.

When enter debug mode, and the code will hang on startup.cm7.s?

My SDK version is the D2203.

I also chech the FlexCAN_ip, also hang on the same condition.

Would you share us the CAN sample code for S32K312 and S32K344?

 

StephenYeh_0-1653904904361.png

 

 

StephenYeh_2-1653905070431.png

 

Tags (1)
0 Kudos
Reply
1 Solution
2,756 Views
namnguyenviet
NXP Employee
NXP Employee

Hello,

As your capture, the code is staying at end_of_eunit_test, which means the example has finished. It's a normal behavior and also proved that there was no problem with the example.

Best Regards,

Nam

View solution in original post

0 Kudos
Reply
2 Replies
2,746 Views
StephenYeh
Contributor III

Hi Nam

Thanks.

Would you share the CAN RX FIFO mode sample code?

0 Kudos
Reply
2,757 Views
namnguyenviet
NXP Employee
NXP Employee

Hello,

As your capture, the code is staying at end_of_eunit_test, which means the example has finished. It's a normal behavior and also proved that there was no problem with the example.

Best Regards,

Nam

0 Kudos
Reply