s32k344 CAN bus sample code hard fault issue.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

s32k344 CAN bus sample code hard fault issue.

ソリューションへジャンプ
2,819件の閲覧回数
StephenYeh
Contributor III

Hi Sir

I will import the sample code s32k344 CAN bus sample code.

When enter debug mode, and the code will hang on startup.cm7.s?

My SDK version is the D2203.

I also chech the FlexCAN_ip, also hang on the same condition.

Would you share us the CAN sample code for S32K312 and S32K344?

 

StephenYeh_0-1653904904361.png

 

 

StephenYeh_2-1653905070431.png

 

タグ(1)
0 件の賞賛
返信
1 解決策
2,799件の閲覧回数
namnguyenviet
NXP Employee
NXP Employee

Hello,

As your capture, the code is staying at end_of_eunit_test, which means the example has finished. It's a normal behavior and also proved that there was no problem with the example.

Best Regards,

Nam

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,789件の閲覧回数
StephenYeh
Contributor III

Hi Nam

Thanks.

Would you share the CAN RX FIFO mode sample code?

0 件の賞賛
返信
2,800件の閲覧回数
namnguyenviet
NXP Employee
NXP Employee

Hello,

As your capture, the code is staying at end_of_eunit_test, which means the example has finished. It's a normal behavior and also proved that there was no problem with the example.

Best Regards,

Nam

0 件の賞賛
返信