s32k312 reset issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

s32k312 reset issue

跳至解决方案
4,280 次查看
NewbieNerd
Contributor IV

Hello, S32K3 team!

First off, thank you for your support with the previous FS26 issue.

I'm now facing a new challenge and seek your assistance.

I've successfully entered the LPOff mode using FS26 on the S32K312.
However, after initiating a reset with a wake-up signal, the board experiences a power reset within about 3 seconds.

When I checked with the Mcu_GetResetReason() function, it appears that the Reset Reason is either 'Power on Reset' or 'HSE boot Failure'.
Despite configuring the clock settings as per the reference manual, as suggested in another post, the reset keeps occurring, independent of my intentions. I’m attaching the log from the UART output for your reference.

I'd greatly appreciate your assistance.
Regard

NewbieNerd_0-1706166040616.pngNewbieNerd_1-1706166175508.png

 

0 项奖励
回复
1 解答
4,205 次查看
NewbieNerd
Contributor IV

Hi  diazmarin09
I resolved the issue by referring to the post.

https://community.nxp.com/t5/S32K/S32K312EVB-reset-problem/m-p/1671141#M24067


And I think It appears that the HSE clock is the problem when creating a sample project in S32DS 3.5.

regard

在原帖中查看解决方案

0 项奖励
回复
2 回复数
4,218 次查看
diazmarin09
NXP TechSupport
NXP TechSupport

Hello NewbieNerd,

I hope all is great with you. Thank you for using the NXP communities.

Is the RSTB pin from the FS26 side asserting periodically? Have you conducted the watchdog refresh before the 256ms timeout? Please refer to the section 22.4 in the FS26 datasheet.

diazmarin09_0-1706902897951.png

 

Regards,

David

0 项奖励
回复
4,206 次查看
NewbieNerd
Contributor IV

Hi  diazmarin09
I resolved the issue by referring to the post.

https://community.nxp.com/t5/S32K/S32K312EVB-reset-problem/m-p/1671141#M24067


And I think It appears that the HSE clock is the problem when creating a sample project in S32DS 3.5.

regard

0 项奖励
回复