s32k148 lwIP without RTOS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

s32k148 lwIP without RTOS

跳至解决方案
5,006 次查看
carl_larsson
Contributor II

Hi!

I am trying to get the lwIP_s32k148 sample project to work without an RTOS. By default, the project uses FreeRTOS and multiple threads. Is there a way to remove the RTOS and run the lwIP sample project on bare metal?

I am using the s32k148evb-q176 and the TJA1101 PHY driver. 

//Calle

0 项奖励
回复
1 解答
4,760 次查看
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi Carl,

The FreeRTOS component can be removed in the newer releases of SDK 3.0.0 and the OS selection in the tcpip component will be updated automatically:

pastedImage_1.png

I hope it helps.

Best Regards,

Diana

在原帖中查看解决方案

0 项奖励
回复
4 回复数
4,761 次查看
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi Carl,

The FreeRTOS component can be removed in the newer releases of SDK 3.0.0 and the OS selection in the tcpip component will be updated automatically:

pastedImage_1.png

I hope it helps.

Best Regards,

Diana

0 项奖励
回复
4,760 次查看
carl_larsson
Contributor II

Thank you! I got it to work with version 3.0.0 of the SDK.

BR

Calle 

0 项奖励
回复
4,760 次查看
naderkhamess
Contributor III

Hello Diana & Carl,

@Diana : first of all i tried to remove FreeRTOS component and it was automatically changed in LWIP into baremetal automatically like you said. However, there is still an error and its unknown. But i want please to know how to ping anyhow,  i have the same board s32k148 and phy_tja1101 and automotive Eth converter fc602. I runned the project phy_tja1101, and LED is green. but in this project there is not tcpip stack. in lwip project i can not ping.pastedImage_1.png

@Carl: could you please let me know how did you ping your board? i have also tja1101, did you just run lwip project and it was working or you had to include TJA1101 Phy driver yourself beside the lwip project? 

0 项奖励
回复
3,923 次查看
jangjeehoon
Contributor I

Please check PHY Reset.

if it's inital value set high, you can ping. 

0 项奖励
回复