11-24-2020
05:33 AM
2,340件の閲覧回数
郑文豪
Contributor I
- 新着としてマーク
- ブックマーク
- 購読
- ミュート
- RSS フィードを購読する
- ハイライト
- 印刷
- 不適切なコンテンツを報告
I disable WDOG_DRV_Trigger(INST_WATCHDOG1) function so that chip can reset by watchdog if timeout.
Code:
/* Including needed modules to compile this module/procedure */
#include "Cpu.h"
#include "clockMan1.h"
#include "pin_mux.h"
#include "watchdog1.h"
#include "pwrMan1.h"
#if CPU_INIT_CONFIG
#include "Init_Config.h"
#endif
volatile int exit_code = 0;
/* User includes (#include below this line is not maintained by Processor Expert) */
#include <stdint.h>
#include <stdbool.h>
/* To use with other board than EVB please comment the following line */
#define EVB
#ifdef EVB
#define LED0 15U
#define LED1 16U
#define LED_GPIO PTD
#else
#define LED0 0U
#define LED1 1U
#define LED_GPIO PTC
#endif
/* Initialize SysTick counter */
void SysTick_Init(void)
{
S32_SysTick->RVR = 0xFFFFFFul;
S32_SysTick->CVR = 0ul;
S32_SysTick->CSR = 0u;
}
/* Enable SysTick counter and interrupt */
void SysTick_Enable(void)
{
S32_SysTick->CSR = S32_SysTick_CSR_TICKINT(1u) | S32_SysTick_CSR_ENABLE(1);
}
/* Disable SysTick */
void SysTick_Disable(void)
{
S32_SysTick->CSR = 0ul;
}
/* SysTick IRQ handler */
void SysTick_Handler(void)
{
/* Variable that stores the number of Watchdog triggers */
static uint8_t s_refreshNumber = 0;
/* After 8 watchdog refreshes, the interrupt will no longer reset the wdog counter */
if(s_refreshNumber <
{
/* Reset Watchdog counter */
// WDOG_DRV_Trigger(INST_WATCHDOG1);
/* Toggle LED0 */
PINS_DRV_TogglePins(LED_GPIO, (1 << LED0));
/* Increment refresh number */
s_refreshNumber++;
}
}
/* WatchDog IRQ handler */
void WDOG_ISR(void)
{
/* Turn off both LEDs */
PINS_DRV_SetPins(LED_GPIO, (1 << LED0) | (1 << LED1));
/* Disable the SysTick timer */
SysTick_Disable();
}
/*!
\brief The main function for the project.
\details The startup initialization sequence is the following:
* - __start (startup asm routine)
* - __init_hardware()
* - main()
* - PE_low_level_init()
* - Common_Init()
* - Peripherals_Init()
*/
int main(void)
{
/* Write your local variable definition here */
/*** Processor Expert internal initialization. DON'T REMOVE THIS CODE!!! ***/
#ifdef PEX_RTOS_INIT
PEX_RTOS_INIT(); /* Initialization of the selected RTOS. Macro is defined by the RTOS component. */
#endif
/*** End of Processor Expert internal initialization. ***/
/* Initialize and configure clocks
* - Setup system clocks
* - Enable clock feed for Ports
* - See Clock Manager component for more info
*/
CLOCK_SYS_Init(g_clockManConfigsArr, CLOCK_MANAGER_CONFIG_CNT,
g_clockManCallbacksArr, CLOCK_MANAGER_CALLBACK_CNT);
CLOCK_SYS_UpdateConfiguration(0U, CLOCK_MANAGER_POLICY_AGREEMENT);
/* Initialize pins
* - Setup output pins for LEDs
* - See PinSettings component for more info
*/
PINS_DRV_Init(NUM_OF_CONFIGURED_PINS, g_pin_mux_InitConfigArr);
/* Stop if the previous reset was caused by the Watchdog */
if(POWER_SYS_GetResetSrcStatusCmd(RCM, RCM_WATCH_DOG) == true)
{
/* Turn on both LEDs */
PINS_DRV_WritePin(LED_GPIO, LED0, 0u);
PINS_DRV_WritePin(LED_GPIO, LED1, 0u);
}
else
{
/* Turn off both LEDs */
PINS_DRV_WritePin(LED_GPIO, LED0, 1u);
PINS_DRV_WritePin(LED_GPIO, LED1, 1u);
/* Install IRQ handlers for WDOG and SysTick interrupts */
INT_SYS_InstallHandler(WDOG_EWM_IRQn, WDOG_ISR, (isr_t *)0);
INT_SYS_InstallHandler(SysTick_IRQn, SysTick_Handler, (isr_t *)0);
/* Enable Watchdog IRQ */
INT_SYS_EnableIRQ(WDOG_EWM_IRQn);
/* Configure and enable SysTick */
SysTick_Init();
SysTick_Enable();
/* Initialize WDOG */
WDOG_DRV_Init(INST_WATCHDOG1, &watchdog1_Config0);
}
while(1)
{
;
}
/*** Don't write any code pass this line, or it will be deleted during code generation. ***/
/*** RTOS startup code. Macro PEX_RTOS_START is defined by the RTOS component. DON'T MODIFY THIS CODE!!! ***/
#ifdef PEX_RTOS_START
PEX_RTOS_START(); /* Startup of the selected RTOS. Macro is defined by the RTOS component. */
#endif
/*** End of RTOS startup code. ***/
/*** Processor Expert end of main routine. DON'T MODIFY THIS CODE!!! ***/
for(;;) {
if(exit_code != 0) {
break;
}
}
return exit_code;
/*** Processor Expert end of main routine. DON'T WRITE CODE BELOW!!! ***/
} /*** End of main routine. DO NOT MODIFY THIS TEXT!!! ***/
/* END main */
/*!
** @}
*/
/*
** ###################################################################
**
** This file was created by Processor Expert 10.1 [05.21]
** for the Freescale S32K series of microcontrollers.
**
** ###################################################################
*/
解決済! 解決策の投稿を見る。
1 解決策
11-25-2020
03:47 AM
2,335件の閲覧回数

NXP TechSupport
- 新着としてマーク
- ブックマーク
- 購読
- ミュート
- RSS フィードを購読する
- ハイライト
- 印刷
- 不適切なコンテンツを報告
Hello,
The interrupt is active only for 128 bus clock cycles and after that the MCU is reset.
It was discussed here:
https://community.nxp.com/t5/S32K/WDOG-direct-reset-does-not-enter-the-interrupt-S32K144/m-p/724793
You can toggle the GPIOs a few times in the ISR and scope the pins.
Regards,
Daniel
1 返信
11-25-2020
03:47 AM
2,336件の閲覧回数

NXP TechSupport
- 新着としてマーク
- ブックマーク
- 購読
- ミュート
- RSS フィードを購読する
- ハイライト
- 印刷
- 不適切なコンテンツを報告
Hello,
The interrupt is active only for 128 bus clock cycles and after that the MCU is reset.
It was discussed here:
https://community.nxp.com/t5/S32K/WDOG-direct-reset-does-not-enter-the-interrupt-S32K144/m-p/724793
You can toggle the GPIOs a few times in the ISR and scope the pins.
Regards,
Daniel