s32k144 CAN example

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
6,791件の閲覧回数
tommysvensson
Contributor II

Hi,

I'm trying to get CAN to work with the evaluation board for S32K144.

 

I have downloaded Design studio and imported examples CAN_MASTER and CAN_SLAVE, (the use S32_SDK_EAR_0.8.1)

 

They build and flash ok.

But I can't see any CAN communication. 

 

I have measured TP20 for sbc_can_rx and TP21 for sbc_can_tx.

TP20 is always low, and TP21 is always high. 

 

What am I missing here?

Think the examples should work out of the box. 

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
4,839件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

do you have EVB board powered by external supply into J16? The SBC chip is powered by this external 12V source.

I tested those demos on 2 EVB and it is working well. There is a same behavior without external power supply.

BR, Petr

元の投稿で解決策を見る

2 返答(返信)
4,840件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

do you have EVB board powered by external supply into J16? The SBC chip is powered by this external 12V source.

I tested those demos on 2 EVB and it is working well. There is a same behavior without external power supply.

BR, Petr

4,839件の閲覧回数
trialaccount12
Contributor V

Hi,

   I have downloaded the S32DS for ARM v2.0.  But I could not find the CAN_MASTER and CAN_SLAVE example in the installed SDK's. I could not find any example for CAN master-slave communication in my folders. 

Can you tell me where am I going wrong in this?

Any pointers would be helpful.

P.S. I wanted to test a simple CAN communication between two S32K144 boards. 

Regards

Ravi

0 件の賞賛
返信