s32k

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
6,397件の閲覧回数
harish89
Contributor II

HI

I am using MC33664 Isolated network high-speed transceiver IC and S32k microcontroller.

Would like to know whether the DATA_RX from MC33664 should be connected to MISO pin of MCU?

 

Thanks

Harish

1 解決策
6,360件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信
4 返答(返信)
6,356件の閲覧回数
harish89
Contributor II

Hi

Thanks for the feedback

Can we get the datasheet of MC33664 updated as it is showing MOSI toward the MCU side for both DATA_TX and DATA_RX

Thanks

Harish

0 件の賞賛
返信
6,367件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Yes, you are correct!

0 件の賞賛
返信
6,363件の閲覧回数
harish89
Contributor II

HI 

Thanks for the feedback.

Also, if i am using any other microcontroller apart from S32K, still we need to connect DATA_RX signal from MC33664 to MISO pin only and DATA_TX to MOSI pin right?

 

Thanks

Harish

タグ(1)
0 件の賞賛
返信
6,361件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Yes correct!

0 件の賞賛
返信