s32k

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决
6,396 次查看
harish89
Contributor II

HI

I am using MC33664 Isolated network high-speed transceiver IC and S32k microcontroller.

Would like to know whether the DATA_RX from MC33664 should be connected to MISO pin of MCU?

 

Thanks

Harish

1 解答
6,359 次查看
guoweisun
NXP TechSupport
NXP TechSupport
0 项奖励
回复
4 回复数
6,355 次查看
harish89
Contributor II

Hi

Thanks for the feedback

Can we get the datasheet of MC33664 updated as it is showing MOSI toward the MCU side for both DATA_TX and DATA_RX

Thanks

Harish

0 项奖励
回复
6,366 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Yes, you are correct!

0 项奖励
回复
6,362 次查看
harish89
Contributor II

HI 

Thanks for the feedback.

Also, if i am using any other microcontroller apart from S32K, still we need to connect DATA_RX signal from MC33664 to MISO pin only and DATA_TX to MOSI pin right?

 

Thanks

Harish

标记 (1)
0 项奖励
回复
6,360 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Yes correct!

0 项奖励
回复