s32K312 MCAL RTE SchM Core Number

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

s32K312 MCAL RTE SchM Core Number

1,212件の閲覧回数
kjy106906
Contributor IV

C:\NXP\SW32K3_S32M27x_RTD_R21-11_5.0.0\eclipse\plugins\Rte_TS_T40D34M50I0R0\include\SchM_Adc.h

The core number is declared as 4 in the file above.
Is there a special reason why it is fixed to 4 and not defined separately for each MCU?
Do I need to change it manually if I use S32K312?

タグ(1)
0 件の賞賛
返信
1 返信

1,115件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @kjy106906,

The define is indicating the maximum core number for the maximal derivative from the family as the memmap files are generic stubs. The actual core number used at runtime is based on the value provided by Osif so it will use the correct core in execution.

danielmartynek_0-1731488690903.pngdanielmartynek_0-1731488690903.png

 

Best regards,

Daniel

0 件の賞賛
返信