s32K312 MCAL RTE SchM Core Number

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

s32K312 MCAL RTE SchM Core Number

1,282 次查看
kjy106906
Contributor IV

C:\NXP\SW32K3_S32M27x_RTD_R21-11_5.0.0\eclipse\plugins\Rte_TS_T40D34M50I0R0\include\SchM_Adc.h

The core number is declared as 4 in the file above.
Is there a special reason why it is fixed to 4 and not defined separately for each MCU?
Do I need to change it manually if I use S32K312?

标记 (1)
0 项奖励
回复
1 回复

1,185 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @kjy106906,

The define is indicating the maximum core number for the maximal derivative from the family as the memmap files are generic stubs. The actual core number used at runtime is based on the value provided by Osif so it will use the correct core in execution.

danielmartynek_0-1731488690903.png

 

Best regards,

Daniel

0 项奖励
回复