placement includes a mix of sections with content error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

placement includes a mix of sections with content error

1,471 Views
vishwadn
Contributor II

Hi,

   I am working on SPI(with DMA) for NAND communication on S32K341 platform. While configuring for DMA, I added Rm module in MCAL and after doing that, I am getting error as "placement includes a mix of sections with content". Please find attachment for error details. Please do let me know how to overcome this error.

0 Kudos
Reply
3 Replies

1,450 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @vishwadn,

I don't see any attachment.

Can you also specify the RTD version?

Do you use S32DS IDE, if so, can you attach the .mex file?

 

Regards,

Daniel

0 Kudos
Reply

1,417 Views
vishwadn
Contributor II

Hi Daniel,

     Please find attached screen shot of error and also .mex file. RTD used is:

SW32K3_RTD_4.4_R21-11_3.0.0_P01_HF02

 

Thanks,

Vishwanath Devara

  

0 Kudos
Reply

1,357 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @vishwadn,

Do you use the compiler specified in the relase notes of the RTD?

And are the compiler options set according the release notes?

 

Thank you,

BR, Daniel

 

0 Kudos
Reply