jlink flash programming S32K344

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

jlink flash programming S32K344

1,281件の閲覧回数
monk_65
Contributor III

 

hello,

 

i use the MR-CANHUBK344 development board with a segger jlink, and i have the same problem of this post

https://community.nxp.com/t5/S32K/S32K344-RTD-PORT-DIO-and-Debugging/td-p/1693264

is the jumper JP1 must be remove to program the board ?

i tried

r0

erase

but it don't work

the file .elf is the demo MR_CANHUBK3_IEEE1722

here the message


Connecting to target via C2
ConfigTargetSettings() start
ConfigTargetSettings() end - Took 24us
InitTarget() start
Unknown SDA AP Id detected: 0xFFFFFFFF
InitTarget() end - Took 2.62ms
Connect failed. Resetting via Reset pin and trying again.
ConfigTargetSettings() start
ConfigTargetSettings() end - Took 13us
InitTarget() start
Unknown SDA AP Id detected: 0xFFFFFFFF
InitTarget() end - Took 1.97ms

 

 

 

 

 

 

 

0 件の賞賛
返信
0 返答(返信)