initial QSPI will be timeout on S32K344 EVB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

initial QSPI will be timeout on S32K344 EVB

3,095 次查看
Jireh
Contributor III

Hi Sir,

 

the QSPI sample code was timeout after called the "Initial Protection" as below.

please help us to check, thanks. 

can we disable this protection function?

Jireh_1-1720170317600.png

we had read this timeout issue.

https://community.nxp.com/t5/S32K/QSPI-FLASH-Init-time-out/m-p/1228072

 

  • SDK: S32DS 3.5 (Build id: 240529 (Update 12)), SDK 4.0.0
  • HW: S32K344 EVB, it was reworked all pins from ENET to QSPI.
  • FW: We used the example code as below.
  • Jireh_0-1720167354576.png

 

thanks.

Jireh

S32K3, @danielmartynek 

0 项奖励
回复
6 回复数

2,603 次查看
Jireh
Contributor III

Hi @VaneB , 

please help,

thanks~

 

  • Trouble:
    • if I used the AutoSAR R21-11 on 344EVB, it still has the TIMEOUT ERROR.
    • But AutoSAR 4.4 was OK as above description P24, D2405.
    • we tested QSPI on S32K344 EVB and complete rework.

 

  • SDK version:
    • AutoSAR: R21-11, P14, D2403.
    • SDK: 3.5.13
    • Jireh_0-1724289879065.png

       

  • Test result: 
    • Status is Busy & timeout in Qspi_Ip_InitProtection()
      • Jireh_1-1724314299056.png

         

    • Status is Busy & timeout in Qspi_Ip_WaitCommandComplete()
      • Jireh_4-1724314498806.png
      • Jireh_0-1724314277258.png

         

    • Status is Busy in Qspi_Ip_CheckMemoryStatus()
      • Jireh_2-1724314330415.png

         

    • Status is Error in Qspi_Ip_ErrorCheck()
      • Jireh_3-1724314360773.png

         

0 项奖励
回复

3,071 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @Jireh 

First of all, hotfix builds are not fully qualified and are not designed for production; replace them with the next qualified standard version. Please test it with the updated SW version.

Did you make any modifications to the example code? With the SW update does it have the same behavior?

 

BR, VaneB

2,991 次查看
Jireh
Contributor III

Hi @VaneB 

 

We changed the sample code to ExFls as below.

Jireh_0-1720535382835.png

but it also had the same timeout problem when initial the protection.

Jireh_1-1720535501667.png

BTW, it always Busy if get the memory status in protection initial.

and then it will be timeout after end of while loop.

why? I didn't change any config.

Jireh_2-1720535877787.png

Jireh_3-1720535915507.png

the attachment is our code.

thanks,

Jireh

0 项奖励
回复

2,928 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @Jireh 

As previously mentioned the hotfix sw versions are not fully qualified, you can download the software versions RTM qualified from S32K3 Standard Software > Automotive SW - S32K3/S32M27x - Real-Time Drivers for Cortex-M.

2,895 次查看
Jireh
Contributor III

Hi @VaneB ,

 

thanks,

we changed to this version and used D2405 sample code, it was working.

But We have a question.

Does the generated codes (in board & generate folder) keep the same between the diff. RTD Dxxxx?

Jireh_0-1721032356906.png

Jireh_1-1721033292742.png

thanks,

Jireh

0 项奖励
回复

2,890 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @Jireh 

Yes, they could be different depending on the RTD version and whether it is compliant with AUTOSAR 4.4 or AUTOSAR R21-11.