[HSE]How to use hse fuction on S32K314

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[HSE]How to use hse fuction on S32K314

930件の閲覧回数
Gideon
Contributor III

Hello,
I'm using S32K314 and I already installed HSE FW(AB swap) successfully.FW version is 1.5.0_2.1.0.

However, during debug application program, it was found that the clock initialization failed when hse is enabled.
Please see screenshot for error details.

Gideon_0-1724313259585.png

 

When debugging another board without hse enabled, the clock can initialize normally.
Please tell me the reason for the failure and how to solve it.

 

0 件の賞賛
返信
1 返信

918件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Seems that caused by S32K3_HSE_BUG_RTD2.0.x

For more detail, please refer to the discussion in Hard fault during hse firmware install

Due to limited resources, we are currently unable to support customers writing from generic email accounts such as gmail.com or qq.com or similar. Please ensure that you use your company email address when communicating with NXP so that we can prioritize your question accordingly. Thank you for your understanding.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信