how to use eeprom quick write mode(flash access error)?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to use eeprom quick write mode(flash access error)?

5,181件の閲覧回数
xieyinghui
Contributor I

Hi, I want to use S32K144 eeprom quick mode to fast writes, call the following API:

void eeprom_write(....){

......

            ret = FLASH_DRV_SetFlexRamFunction(&flashSSDConfig, EEE_QUICK_WRITE, 128, NULL);

            while ((FTFC->FCNFG & FTFC_FCNFG_EEERDY_MASK) == 0);

            ret = FLASH_DRV_EEEWrite(&flashSSDConfig, relAddr, 124, src);

......

}

when i call eeprom_write this function the second time, FSTAT register 5 bit will set 1 (flash access error), why?

タグ(1)
0 件の賞賛
返信
8 返答(返信)

5,040件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi [email protected],

If the FlexRAM is set for a 128-byte quick write.

You need to write exactly 128 bytes in the FlexRAM, not 124 bytes.

BR, Daniel

0 件の賞賛
返信

5,040件の閲覧回数
xieyinghui
Contributor I

Hi Daniel,

when i write 128 bytes in the FlexRAM, i find eeprom quick write don't work. It looks like normal mode.

 

when i  call the API(eeprom_write) this way, only 384(3*128)bytes is fast write mode, more data will be normal mode, if I want to use fast mode, what should I do?

ret = FLASH_DRV_SetFlexRamFunction(&flashSSDConfig, EEE_QUICK_WRITE, 0x200u, NULL); //This function is called only once

void eeprom_write(....) //Call this function multiple times to write 128bytes each time

{

......

            while ((FTFC->FCNFG & FTFC_FCNFG_EEERDY_MASK) == 0);

            ret = FLASH_DRV_EEEWrite(&flashSSDConfig, relAddr, 128, src);

......

}

0 件の賞賛
返信

5,040件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi [email protected],

When you call this:

FLASH_DRV_SetFlexRamFunction(&flashSSDConfig, EEE_QUICK_WRITE, 0x200u, NULL);

you need to write exactly 512 bytes.

If you want to write next 512 bytes after the first write, call the function again

FLASH_DRV_SetFlexRamFunction(&flashSSDConfig, EEE_QUICK_WRITE, 0x200u, NULL);

And write 512 bytes again.

Regards,

Daniel

0 件の賞賛
返信

5,040件の閲覧回数
xieyinghui
Contributor I

Hi Daniel,

when i call this way:

void eeprom_write(....){

......

            ret = FLASH_DRV_SetFlexRamFunction(&flashSSDConfig, EEE_QUICK_WRITE, 128, NULL);

            while ((FTFC->FCNFG & FTFC_FCNFG_EEERDY_MASK) == 0);

            ret = FLASH_DRV_EEEWrite(&flashSSDConfig, relAddr, 128, src);

......

}

I've found that using this quick mode doesn't work

0 件の賞賛
返信

5,040件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi [email protected],

What exactly does not work?

I have tested your code in the flash_partitioning_s32k144 SDK example:

pastedImage_3.png

pastedImage_2.png

The FTFC module didn't report any error.

After power-cycling the MCU, I can see all the data in FlexRAM.

pastedImage_6.png

Regards,

Daniel

0 件の賞賛
返信

5,040件の閲覧回数
xieyinghui
Contributor I

Hi Daniel:

I know I can write the data in, but the writing speed is the same as normal mode.

In normal mode, The 128bytes I tested are 12~13ms, and the 128bytes I tested in the fast mode you gave me are also 12~13ms. Is this reasonable?

start_time = k_cycle_get_32();

ret = FLASH_DRV_SetFlexRamFunction(&flashSSDConfig, EEE_QUICK_WRITE, len, NULL);
__ASSERT_NO_MSG(STATUS_SUCCESS == ret);
while ((FTFC->FCNFG & FTFC_FCNFG_EEERDY_MASK) == 0);
ret = FLASH_DRV_EEEWrite(&flashSSDConfig, relAddr, len, src);  //len = 128;
stop_time = k_cycle_get_32();
cycles_spent = stop_time - start_time;
ms_spent = cycles_spent / sys_clock_hw_cycles_per_tick();
LOG_INF("eeprom write info: cycles_spent = %d, ms_spent = %d", cycles_spent, ms_spent);

The print information is as follows:

eeprom write info: cycles_spent = 999628, ms_spent = 12    //ms_spent is for how much ms

Looking forward to your reply;

0 件の賞賛
返信

5,040件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi [email protected],

Please have a look at the S32K1xx datasheet, rev13, Table 35.

pastedImage_2.png

pastedImage_3.png

You can estimate the max. execution time for 128B of normal writes and 128B of quick writes (including the cleanup after the last write).

AN11983 Using the S32K1xx EEPROM Functionality

pastedImage_2.png

The code that posted measures not only the execution time of the quick writes but the SetFlexRAM function and the SW overhead of the driver as well.

Regards,

Daniel

0 件の賞賛
返信

5,040件の閲覧回数
xieyinghui
Contributor I

Hi Daniel,

when i call this way:

void eeprom_write(....){

......

            ret = FLASH_DRV_SetFlexRamFunction(&flashSSDConfig, EEE_QUICK_WRITE, 128, NULL);

            while ((FTFC->FCNFG & FTFC_FCNFG_EEERDY_MASK) == 0);

            ret = FLASH_DRV_EEEWrite(&flashSSDConfig, relAddr, 128, src);

......

}

0 件の賞賛
返信