l want to set 4k pflash bytes to save data, and set 4k dflash to save data. For example ,there are
"uint8_t p_flash_data1[1024]" and "uint8_t p_flash_data1[3072]",now l want to set "app_data" to save p_flash_data1[512] and p_flash_data2 [512] .who can tell me how to change the"s32k1xx_flash.id" ,thank you for you response.
below is the "s32k1xx_flash.id" code.
MEMORY
{
/* Flash */
m_interrupts (RX) : ORIGIN = 0x00000000, LENGTH = 0x00000400
m_flash_config (RX) : ORIGIN = 0x00000400, LENGTH = 0x00000010
m_text (RX) : ORIGIN = 0x00000410, LENGTH = 0x00008000-0x410
app_data (RW) : ORIGIN = 0X00008000, LENGTH = 0X1000; /* I add 4k bytes memory to save data */
ccp_data (RW) : ORIGIN = 0x10000000, LENGTH = 0X1000; /* I add 4k bytes memory to save ccp data */
/* SRAM_L */
m_data (RW) : ORIGIN = 0x1FFF8000, LENGTH = 0x00008000
/* SRAM_U */
m_data_2 (RW) : ORIGIN = 0x20000000, LENGTH = 0x00007000
}
解決済! 解決策の投稿を見る。
Hi,
You don't have to have data_app, data_app1, data_app2 if you put them all into one section (app_data).
I do not understand what do you intend to do with the pragma.
Regards,
Daniel
Hi,
In c. file create your array:
__attribute__ ((section(".data_app"))) uint8_t p_flash_data1[1024] = {1,2,3,4,5};
Then in the linker file put .data_app into app_data section.
Write it just after m_text section.
…
} > m_text
.data_app :
{
. = ALIGN(4);
KEEP (*(.data_app))
. = ALIGN(4);
} > app_data
Similarly for ccp_data memory section.
Regards,
Daniel
Daniel, l am very thank for you response firstly.
if l have "uint8 p_flash_data1[1024]" and "uint8
uint16 p_flash_data2[128]" and "uint32 p_flash_data3[256]" now,l want save it in "app_data" memory,please check my code to response my setting is right or wrong ,thank you,Daniel.
below is the code,
p_flash_data1[1024] memory is 0x00008000 to 0x000083ff,
p_flash_data4 to p_flash_data259 memory is 0x00008400 to 0x000084ff,
p_flash_data2[128] memory is 0x00008500 to 0x000086ff,
p_flash_data3[128] memory is 0x00008700 to 0x00008aff
in link file , below code setting is to trouble ,whether is any simple setting,for example,if use "#pragme" to set it,please give me the way to set it. thank you
__attribute__ ((section(".data_app"))) uint8_t p_flash_data4 ;
_attribute__ ((section(".data_app"))) uint8_t p_flash_data5 ;
...
_attribute__ ((section(".data_app"))) uint8_t p_flash_data259 ;
in .c file
__attribute__ ((section(".data_app"))) uint8_t p_flash_data4 ;
__attribute__ ((section(".data_app"))) uint8_t p_flash_data5 ;
__attribute__ ((section(".data_app"))) uint8_t p_flash_data259 ;
__attribute__ ((section(".data_app2"))) uint16_t p_flash_data3[100] = {1,2,3,4,5};
in link file
.data_app1 : { . = ALIGN(2); KEEP (*(.data_app1)) . = ALIGN(2); } > app_data
.data_app2 : { . = ALIGN(4); KEEP (*(.data_app2)) . = ALIGN(4); } > app_data
Hi,
You don't have to have data_app, data_app1, data_app2 if you put them all into one section (app_data).
I do not understand what do you intend to do with the pragma.
Regards,
Daniel
Daniel, l am very thank for you response firstly.
if l have "uint8 p_flash_data1[1024]" and "uint16 p_flash_data2[100]" and "uint32 p_flash_data1[100]" now,l want save it in "app_data" memory,please check my code to response my setting is right or wrong ,thank you,Daniel.
in .c file
__attribute__ ((section(".data_app"))) uint16_t p_flash_data3[100] = {1,2,3,4,5};
in link file
.data_app :
{
. = ALIGN(4);
KEEP (*(.data_app))
. = ALIGN(4);
} > app_data