S32K mass program tools

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K mass program tools

ソリューションへジャンプ
5,426件の閲覧回数
hansonhe
NXP Employee
NXP Employee

Dear,

As we known, we could use IAR or S32DS for S32K debug and download, whether we have some offline GUI or USB standalone tools for firmware downloading, it is only program update without debug, such as Segger company J-Flash software for cortex M0, M3, M4.

0 件の賞賛
返信
1 解決策
4,797件の閲覧回数
hansonhe
NXP Employee
NXP Employee

Dear, we have closed by ourselves, now Segger could support S32K144.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
4,797件の閲覧回数
songhanson
Contributor I

Hi Hanson,

可以使用Segger的Flasher,目前JFlash已经支持S32K的下载,JFlash配置好目标芯片S32K后,然后选择download到Flasher中,然后按下按键即可对目标芯片离线烧写。

1.png

或者参考我的iFlasher:

MiniFlasherS.jpg

具体描述:

MiniFlasher | Thanks For Everything. 

0 件の賞賛
返信
4,797件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Is this How To Program the Application in the Flash/RAM what you are looking for ?

The program is called RAppID_BL and is available here

Best regards,
Daniel

0 件の賞賛
返信
4,797件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

could you please clarify your question? From your post I am not sure what are you asking for.

Regards,

Martin

0 件の賞賛
返信
4,797件の閲覧回数
hansonhe
NXP Employee
NXP Employee

Dear, we have closed by ourselves, now Segger could support S32K144.

0 件の賞賛
返信