first defined here ERORR while compling s32k144 code in S32DS 3.5

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

first defined here ERORR while compling s32k144 code in S32DS 3.5

3,734件の閲覧回数
steven_zhang
Contributor V

I created a Adc test project for K144 in S32DS 3.5 ,GOT many first defined here  errors in the .c docs.

how to fix it.

 

FLASH/../SDK/S32K144_SDK_4.0.1/platform/drivers/src/interrupt/interrupt_manager.c:225: first defined here

 

16:58:40 Build Failed. 53 errors, 0 warnings. (took 11s.930ms)

 

 

0 件の賞賛
返信
4 返答(返信)

3,716件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

did you created your project from a scratch (File -> New S32DS Application Project) or from SDK example? 

 

If from scratch - after adding all modules and configuration - did you run Update Code in configuration tool? 

jiri_kral_0-1663673499681.pngjiri_kral_0-1663673499681.png

 

Jiri

 

0 件の賞賛
返信

3,700件の閲覧回数
steven_zhang
Contributor V

I created my project from a scratch (File -> New S32DS Application Project). after i added adc moudule to the project ,i clicked the update button. 

0 件の賞賛
返信

3,692件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

can you please share full output from build console? 

0 件の賞賛
返信

3,689件の閲覧回数
steven_zhang
Contributor V

the attachment doc is the full  output。

0 件の賞賛
返信