S32K144EVB D3(Diode) Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144EVB D3(Diode) Error

2,759 Views
gksn284
Contributor I

D3 Diode and RGB LED are turn off.

D1 Diode(near the reset button) is turn on(green and no blink)

2.jpg
 

I tried updating the Bootloader Mode.

But I don't know what is the problem.

 

I have a Universal Multilink FX High-Speed Development Interface.

Please somebody help me!

0 Kudos
Reply
5 Replies

2,747 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@gksn284

If D3 is not turned on ,it measn there may be a problem with your power supply. 

Senlent_0-1664155579289.png

You can try to use external 12V power supply,this might be useful, and don't forget the J107 should be changed to 1-2.

0 Kudos
Reply

2,733 Views
gksn284
Contributor I

First, Thank you for your answer!

As you said, I connected the 12V power supply.

But there's no light, there's only heat. (I am aware that J107 should be changed to 1-2)

 

So I measured the voltage myself. (J107 : 2-3, microusb cable)

KakaoTalk_20220926_163728887_02.jpg

↑J107 : 2-3 unpluged

KakaoTalk_20220926_163728887_01.jpg

↑J107 : 2-3 pluged

KakaoTalk_20220926_163728887.jpg

↑ TP9's voltage

 

I think there's a reason why the voltage drops as it connects.

Do you have any guesses?

0 Kudos
Reply

2,730 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@gksn284

Do you know which specific heating chip is? Is it U15? According to the measurement results, there should be no problem with P5V_SBC. It is very likely that there is a problem with the U15. This is my guess.

0 Kudos
Reply

2,718 Views
gksn284
Contributor I
 

There is heating near the power connection. (12V)

If there is a problem with u15, can I fix it myself?

Or Should  I go to the repair shop?

14.PNG

0 Kudos
Reply

2,704 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@gksn284

If there is a problem with the U15, you can only replace this chip, it is not easy to repair.

0 Kudos
Reply