event occured timing is varies in eMIOS MCB mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

event occured timing is varies in eMIOS MCB mode

跳至解决方案
1,099 次查看
Aren
Contributor II

I use eMIOS UC23 as MCB mode.

CORE Clock : 100MHz
prescaler : all "1"
UC23 A register : 5000

I am checking flag interrupts with an oscilloscope, but the timing of event occurrences varies.

Please let me know if there are any possible causes for variation.

#s32k

标记 (1)
0 项奖励
回复
1 解答
1,026 次查看
Aren
Contributor II
There was a problem with the core clock. I reviewed the clock settings and the problem was resolved.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,027 次查看
Aren
Contributor II
There was a problem with the core clock. I reviewed the clock settings and the problem was resolved.
0 项奖励
回复
1,068 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@Aren

Could you provide your demo project and test details, we will take the time to help you check it.

0 项奖励
回复
1,086 次查看
Aren
Contributor II

A note about variability

I want an event to occur every 50us, but the events occur at completely different times, such as 10us, 20us, etc.

0 项奖励
回复