event occured timing is varies in eMIOS MCB mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

event occured timing is varies in eMIOS MCB mode

ソリューションへジャンプ
1,106件の閲覧回数
Aren
Contributor II

I use eMIOS UC23 as MCB mode.

CORE Clock : 100MHz
prescaler : all "1"
UC23 A register : 5000

I am checking flag interrupts with an oscilloscope, but the timing of event occurrences varies.

Please let me know if there are any possible causes for variation.

#s32k

タグ(1)
0 件の賞賛
返信
1 解決策
1,033件の閲覧回数
Aren
Contributor II
There was a problem with the core clock. I reviewed the clock settings and the problem was resolved.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,034件の閲覧回数
Aren
Contributor II
There was a problem with the core clock. I reviewed the clock settings and the problem was resolved.
0 件の賞賛
返信
1,075件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@Aren

Could you provide your demo project and test details, we will take the time to help you check it.

0 件の賞賛
返信
1,093件の閲覧回数
Aren
Contributor II

A note about variability

I want an event to occur every 50us, but the events occur at completely different times, such as 10us, 20us, etc.

0 件の賞賛
返信