emios trigger

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

emios trigger

Jump to solution
1,558 Views
Ayaz
Contributor IV

Hi

I am trying to test the system so that the BCTU is triggered via PWM  at every flag generation. I would like to plot the flag that triggers the BCTU on an oscilloscope. How do I do that?

I am trying to get the generating emios_pwm flag outputted on an oscilloscope, by using the EMIOS_PWM_IP_INTERRUPT_REQUEST callback function, but i am not sure the interrupt for EMIOS is working. I have attached the project below

RTD 4.00

S32K344 T172

Tags (1)
0 Kudos
Reply
1 Solution
1,531 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@Ayaz

This is a demo i made before and the RTD version is 2.0.3, maybe you can refer to it.

View solution in original post

1 Reply
1,532 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@Ayaz

This is a demo i made before and the RTD version is 2.0.3, maybe you can refer to it.