eMcem_Init() return is E_NOT_OK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

eMcem_Init() return is E_NOT_OK

Jump to solution
3,723 Views
Sylvia_jiang
Contributor IV

I am working on the EVB Q172 with testing EIM/ERM in example code SPD_101_S32K344, Bist/eMcem/SafetyBase modules imported keep defaults. I find NCF_S0 value is always is 1 in debugging eMcem_Init(). What shall I do to clear NCF0 fault and have eMcem_Init() performed successfully?

 

0 Kudos
Reply
1 Solution
3,695 Views
cuongnguyenphu
NXP Employee
NXP Employee

Hi,
I found a demo project in S32K3 SPD 1.0.2 in below link:
 https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&element=14032037

This demo use eMcem_Init() successfully, so you can refer to it

View solution in original post

0 Kudos
Reply
3 Replies
3,696 Views
cuongnguyenphu
NXP Employee
NXP Employee

Hi,
I found a demo project in S32K3 SPD 1.0.2 in below link:
 https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&element=14032037

This demo use eMcem_Init() successfully, so you can refer to it

0 Kudos
Reply
3,136 Views
Sjoshi11
Contributor I
Hi, the link you've given looks useful to me. but I am not able to access it. It is redirecting me to login page again and again. could you give some code snippet or a different link which might work?
0 Kudos
Reply
3,111 Views
cuongnguyenphu
NXP Employee
NXP Employee
0 Kudos
Reply