eMcem_Init() return is E_NOT_OK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

eMcem_Init() return is E_NOT_OK

ソリューションへジャンプ
3,686件の閲覧回数
Sylvia_jiang
Contributor IV

I am working on the EVB Q172 with testing EIM/ERM in example code SPD_101_S32K344, Bist/eMcem/SafetyBase modules imported keep defaults. I find NCF_S0 value is always is 1 in debugging eMcem_Init(). What shall I do to clear NCF0 fault and have eMcem_Init() performed successfully?

 

タグ(1)
0 件の賞賛
返信
1 解決策
3,658件の閲覧回数
cuongnguyenphu
NXP Employee
NXP Employee

Hi,
I found a demo project in S32K3 SPD 1.0.2 in below link:
 https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&element=14032037

This demo use eMcem_Init() successfully, so you can refer to it

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,659件の閲覧回数
cuongnguyenphu
NXP Employee
NXP Employee

Hi,
I found a demo project in S32K3 SPD 1.0.2 in below link:
 https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&element=14032037

This demo use eMcem_Init() successfully, so you can refer to it

0 件の賞賛
返信
3,099件の閲覧回数
Sjoshi11
Contributor I
Hi, the link you've given looks useful to me. but I am not able to access it. It is redirecting me to login page again and again. could you give some code snippet or a different link which might work?
0 件の賞賛
返信
3,074件の閲覧回数
cuongnguyenphu
NXP Employee
NXP Employee
0 件の賞賛
返信