design studio error difference

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

design studio error difference

1,446 Views
Hoon
Contributor III

Two projects were created using the same source code. However, the same error appears as warning in one project but error in the other, so it is not built. I compared the two because I thought it was a difference in the combiner setting, but I could not confirm the difference. Is there a way to solve this problem?

 

 

 

0 Kudos
Reply
2 Replies

1,410 Views
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @Hoon , 

 

Please can you provide more information to help to understand the issue, the screenshots for the error and warning you are getting.  

 

And also you can also attach the log from the workspace : 

S32DS workspace:  C:\Users\Public\[workspace_name]\.metadata ( or wherever you workspace is located) 

 

Thank you.

 

Best regards.

 

 - Mehul Patel  

 

 

0 Kudos
Reply

1,373 Views
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @Hoon , 

 

Please let us know any further update on the case. 

 

Please can you share the log. 

 

Thank you. Best regards. 

 

-Mehul Patel

0 Kudos
Reply