code hangs on WDOG_EWM_IRQHandler()

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

code hangs on WDOG_EWM_IRQHandler()

ソリューションへジャンプ
3,059件の閲覧回数
s32k146_ige
Contributor IV

My code has started to hang in WDOG_EWM_IRQHandler (), it was working while ago. there is apparent no reason to have this behavior. 

I have 2 freertos task running, if i disable task 2, it runs fine and doesnt hang in default ISR. But if i enable task 2 it hangs, in task 2 i have added 10ms delay at very start. and while single stepping this vTaskdelay sends the code in default ISR

static void task2()
{
	uint32_t lu32Counter = 0;
	// wait 10ms
	vTaskDelay(pdMS_TO_TICKS(10));

I have 2 interrupt running 1 for uart1 and 1 for uart2. apart from that i wanted to use GPIO interrupt but it is disabled now. 

I also added following code to disable WDOG, at start

I have also tried increasing the TASK stack depth and had no effect

  WDOG->CNT=0xD928C520;     /* Unlock watchdog 		*/
  WDOG->TOVAL=0x0000FFFF;   /* Maximum timeout value 	*/
  WDOG->CS = 0x00002100;    /* Disable watchdog 		*/

can anyone guide me in diagnosing this fault ?

 

 

タグ(2)
0 件の賞賛
返信
1 解決策
3,037件の閲覧回数
s32k146_ige
Contributor IV

Hi, There is no other ISR used other than UART1 and 2. But this problem was persistent. After lots of effords we decided to create new workspace and it worked in new WS.

this is kinda illogical situation because code was not edited. same code with same stack size worked after importing in new workspace.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,044件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Sushant Naik,

The Default_ISR is probably a fault exception, I assume you don't have HardFault_Handler() implemented in the project.

Can you confirm it by reading the CFSR core register in the Default_ISR and debug it?

You should be able to find the type of the exception and the PC address of the fault instruction.

https://community.nxp.com/t5/S32K-Knowledge-Base/Fault-handling-on-S32K14x/ta-p/1114447

 

Thank you,

BR, Daniel

 

0 件の賞賛
返信
3,038件の閲覧回数
s32k146_ige
Contributor IV

Hi, There is no other ISR used other than UART1 and 2. But this problem was persistent. After lots of effords we decided to create new workspace and it worked in new WS.

this is kinda illogical situation because code was not edited. same code with same stack size worked after importing in new workspace.

0 件の賞賛
返信