When importing the NXP example S32K144_PT2000_EXAMPLE into S32DS2.2, GCC error occur.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

When importing the NXP example S32K144_PT2000_EXAMPLE into S32DS2.2, GCC error occur.

ソリューションへジャンプ
2,918件の閲覧回数
ALEX_W
Contributor II

When importing the official NXP example S32K144_PT2000_EXAMPLE into S32DS2.2 according to the NXP official manual using the FRDMPKPT2000EVM evaluation board, GCC and makefile issues occurred. The specific error messages are shown in the following figures

.

0 件の賞賛
返信
1 解決策
2,820件の閲覧回数
ALEX_W
Contributor II

I have independently solved the problem that the S32K144_PT2000_EXAMPLE cannot be compiled normally. Please follow the steps in the figure below to solve it.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,821件の閲覧回数
ALEX_W
Contributor II

I have independently solved the problem that the S32K144_PT2000_EXAMPLE cannot be compiled normally. Please follow the steps in the figure below to solve it.

0 件の賞賛
返信
2,888件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please refer to the discussion in S32DS S32K144_PT2001_EXAMPLE errors.

Hope it helps.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
2,849件の閲覧回数
ALEX_W
Contributor II

Hi, Robin!

I have strictly followed the operational matters in the link you sent me, but the problem still hasn't been solved and there are still error warnings. I have attached the picture below for your reference.

 

Best Regards,
Alex

0 件の賞賛
返信