When ConfigureAdvancedSecureBoot, the HSE_MU_GetHseStatus value is always the same.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

When ConfigureAdvancedSecureBoot, the HSE_MU_GetHseStatus value is always the same.

1,000件の閲覧回数
squirrel_rin
Contributor I

Dear All.

Debugging with ConfigureAdvancedSecureBoot.
If InstallSMR or HSE_InstallCoreResetEntry is successful, the secure boot related bit is not toggled when HSE status is retrieved.
(However, it is normal when ConfigureSHESecurureBoot is used.)
Is this behavior intended? Why not support ConfigureAdvancedSecureBoot?

 

0 件の賞賛
返信
1 返信

965件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @squirrel_rin 

different status bits are used for SHE secure boot and Advanced secure boot. Isn't that the problem? From Secure boot app note:

lukaszadrapa_0-1720524792440.pnglukaszadrapa_0-1720524792440.png

Regards,

Lukas

0 件の賞賛
返信