When ConfigureAdvancedSecureBoot, the HSE_MU_GetHseStatus value is always the same.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

When ConfigureAdvancedSecureBoot, the HSE_MU_GetHseStatus value is always the same.

1,014 Views
squirrel_rin
Contributor I

Dear All.

Debugging with ConfigureAdvancedSecureBoot.
If InstallSMR or HSE_InstallCoreResetEntry is successful, the secure boot related bit is not toggled when HSE status is retrieved.
(However, it is normal when ConfigureSHESecurureBoot is used.)
Is this behavior intended? Why not support ConfigureAdvancedSecureBoot?

 

0 Kudos
Reply
1 Reply

979 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @squirrel_rin 

different status bits are used for SHE secure boot and Advanced secure boot. Isn't that the problem? From Secure boot app note:

lukaszadrapa_0-1720524792440.png

Regards,

Lukas

0 Kudos
Reply