What the relationship between message buffer and RX Fifo in FlexCAN of s32k144?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What the relationship between message buffer and RX Fifo in FlexCAN of s32k144?

2,290 Views
victor_song_171
Contributor III

What the relationship between message buffer and RX Fifo in FlexCAN of s32k144?

If i want recieve can data with filter(specified id recieved) in can interrupr, which one shall configed?

Is there any example about config can interrupt recieving?


Any reply with my thanksfull.

0 Kudos
Reply
1 Reply

2,136 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

the MB can be configured for both receive or transmit operation, supporting both the classical CAN and CAN FD frames. RXFIFO is capable to receive only classical CAN frames and has storage capacity for up to six frames. DMA can be used to read messages from RXFIFO. The RXFIFO should not be used when CAN FD feature is enabled. Once RXFIFO is enabled, it uses memory area that is normally occupied by MBs. The number of "unavailable" MBs depends on RXFIFO ID filter table length. I suggest to read chapters 53.4.3 - 53.4.6 of the device RM to fully understand the MB and RXFIFO structure.

See attached main.c I modified to add RX interrupt to the FlexCAN_S32K144 demo example available in the S32 Design Studio. This example is using dedicated MB for message receiving.

BR,

Petr

0 Kudos
Reply