Hello,
The RM 12.1 describes this in the section "39.4.5 Peripheral Doze".
Several peripherals support Peripheral Doze mode. In this mode, a register field can be used to disable the peripheral for the duration of a low-power mode.
So, for example, LPSPI operation can continue operating in stop mode if the Doze Enable bit (CR[DOZEN]) is clear and the LPSPI is using an external or internal clock source that remains operating during stop mode.
Otherwise when the DOZEN bit is set the LPSPI is disabled for the duration of a stop mode.
This question has been already discussed in these community threads:
How is the Doze mode working in S32K series
Low power and Doze Mode question in S32K
I hope it helps.
Best regards,
Diana
Hello,
The RM 12.1 describes this in the section "39.4.5 Peripheral Doze".
Several peripherals support Peripheral Doze mode. In this mode, a register field can be used to disable the peripheral for the duration of a low-power mode.
So, for example, LPSPI operation can continue operating in stop mode if the Doze Enable bit (CR[DOZEN]) is clear and the LPSPI is using an external or internal clock source that remains operating during stop mode.
Otherwise when the DOZEN bit is set the LPSPI is disabled for the duration of a stop mode.
This question has been already discussed in these community threads:
How is the Doze mode working in S32K series
Low power and Doze Mode question in S32K
I hope it helps.
Best regards,
Diana